5/7/2015 7:58 PM | |
Joined: 2/8/2015 Last visit: 4/15/2024 Posts: 462 Rating: (8) |
Hi. Is there HOT restart functionality for S7-1500 system? Thanks |
5/8/2015 12:56 AM | |
Joined: 11/29/2011 Last visit: 4/24/2024 Posts: 1354 Rating: (229) |
Hi, OB101 is not supported in S7-1500. See here: Which organization blocks (OBs) can you not migrate from the S7-300/400 to the S7-1500? What do you need to do? Almost complete user program Retentivity is achievable with optimized DBs. So with a well structured code an "almost" hot start should be doable... Cheers |
Last edited by: MicroMan at: 5/8/2015 1:08:30 AMLast edited by: MicroMan at: 5/8/2015 1:11:55 AM- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
Follow us on