Industry Online Support
Technical Forum
12/19/2007 6:52 AM | |||||||||||||||||||||||||||||||
Posts: 25 Rating: (3) |
Dear Experts, I have data from PCS7 AS to be transferred to an OfficePC Which has only OPC Scout but no WinCC/Data Bridge etc., A PC station is configured in that Office PC Using the NCM PC manager and an OPC connection configured with AS using netpro. The OPC scout Shows all the data from the AS in the OPC.Simatic Net Server. Now, i have to export the data from OPC Scout to an Excel file. So i downloaded an example code From Siemens net through the ID. http://support.automation.siemens.com/WW/view/en/24299099 Fortunately, It Shows the values in the format and im able to read/ Write values.
How can i do it?? Its Very Very Urgent. Any body expert in VB can help or is there any other easy method?? Thankyou, VishnuKarthick. AttachmentOPCClient.zip (742 Downloads) |
||||||||||||||||||||||||||||||
Follow us on