5/6/2015 1:48 PM | |
Posts: 46 Rating: (3) |
Hi, these are quite a lot of questions to answer. Well first I would recommend to have a look at the following application example which explains the basics: In your configuration you need a DP/PA-coupler which is connected to the DP-interface of the CPU. On the PA-side of the coupler you insert your PA-device Furthermore there is also a chapter in the PCS7 compendium describing how to integrate field devices (chapter 5.7) Regarding CFC there is also a manual describing the basics:
Hope this helps to answer the basic questions ... |
5/7/2015 11:49 AM | |
Posts: 14 Rating: (0) |
Thank you so much for helping. I have another problem regarding the communication from PC to S7-400. Could you explain on what to do? (Refer Picture Attached) |
5/7/2015 12:17 PM | |
Posts: 46 Rating: (3) |
probably the wrong PG/PC interface ... Have you tried the other ones already? |
5/20/2015 12:34 PM | |
Posts: 14 Rating: (0) |
Hi, I have a few of PROFIBUS PA instruments in my plant. Is it okay if it is in DP-Norm, it doesn't show the graphics of the instruments. What do I need to do? |
Follow us on