1/5/2015 12:13 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
Do you have the option to write in SCL or only ladder, STL? |
1/5/2015 12:25 AM | |
Joined: 10/23/2014 Last visit: 3/25/2024 Posts: 201 Rating: (0) |
only ladder |
1/5/2015 12:46 AM | |
Joined: 10/23/2014 Last visit: 3/25/2024 Posts: 201 Rating: (0) |
thank you for your efforts with me but the program is not written by ladder language i can not understand it exactly |
5/14/2015 9:10 AM | |
Joined: 10/23/2014 Last visit: 3/25/2024 Posts: 201 Rating: (0) |
if i use cp 341 what is the function will be used to receive data in ladder diagram? |
5/21/2015 11:03 PM | |
Joined: 10/23/2014 Last visit: 3/25/2024 Posts: 201 Rating: (0) |
where can I connect two wires of RS 422 which come from gyro to cp 341? |
Follow us on