5/31/2015 3:05 PM | |
Posts: 7 Rating: (0) |
Hello everyone, I would like its aid to solve a problem on my network when I insert a new hardware. I have a CPU 315-2 in slave configuration on my network, I need to enter my network in one INTECONT balance of Schenck when I insert the gsd of Schenck, my CPU-315-2 is in and out of the network (SF LED ALWAYS ON E BF LED FLASHING) hYQswY.jpg - (In this situation my network is ok, not yet inserted the GSD module Schenck) When I insert the new GSD (Device Adress 71), all my hardware on the network continue to network with the exception of my CPU-315-2 (Device Adress 70) - w5Mmnr.jpg To try to find out what led my cpu 315-2 this situation, I accessed your diagnostic buffer on module information , the message she shows me is this: sXezbZ.jpg EWYNSd.jpg When I take INTECONT GSD (Device Adress 71) of my network, my CPU 315-2 returns to its normal operation ... I've tried different way to work around this problem, but to no avail; I thank the help of all AttachmentBleeding_Edge.zip (179 Downloads) |
Last edited by: CS Moderator at: 6/2/2015 1:10:58 PMpictures as attachment |
|
6/1/2015 3:01 PM | |
Posts: 7 Rating: (0) |
This, are in same line Profibus... I made a simple drawing of the topology of my network... |
6/1/2015 4:31 PM | |
Posts: 7 Rating: (0) |
Well, I did a test and I changed my 1.5Mbps speed to 500 Kbps and continued in the same way, would have some other test to be done? |
Follow us on