6/1/2015 4:15 PM | |
Joined: 3/2/2015 Last visit: 4/18/2024 Posts: 3 Rating: (0) |
Hello, I'm trying to use an RFID system RF180C (+ RF210R) with an S7-300 CPU. According to the manual under (oct 2014), with my configuration I need to use the Ident Profile instead of the Ident blocks (both included in the folder "Optional package" of Tia Portal V13 SP1). Does anyone know if it is now possible to use the Ident blocks because there are easy to use? The Ident profile is more complicated to understand and I would like to avoid it. Thank you very much for your help. Best regards. Pascal https://cache.industry.siemens.com/dl/files/029/106368029/att_33071/v1/FH_Ident-Profil_76_en-US.pdf |
Last edited by: U_76d7ce36-b7a1-4512-af09-b04996691d23 at: 6/1/2015 4:16:19 PM |
|
6/1/2015 5:21 PM | |
Joined: 10/1/2013 Last visit: 4/17/2024 Posts: 605 Rating: (71) |
Hi, there is no need for using the ident profile itself. The ident blocks (which consist of the ident profile) work fine. There is just one thing you have to care about: The reset block. In your case you have to use the special "Reset_RF200" block. Just give it a try... regards,
/Edit: /Edit2:
|
Last edited by: Owei at: 6/1/2015 5:23:08 PMLast edited by: Owei at: 6/1/2015 5:36:20 PM |
|
Follow us on