6/11/2015 2:51 PM | |
Joined: 12/22/2014 Last visit: 10/7/2021 Posts: 173 Rating: (23) |
Hi I think the answer is yes and no. It is possible to connect non-PCS7 systems to the maintenance station using e.g. SNMP. However this will give you the possibility to add CPU's and Remote IO to the Maintenance Station. As I see it, it is only possible to add normal AS configurations if they are part of a PCS7 project.
Attached is the manual with the instructions for implementing a Maintenance Station. AttachmentPCS7_MaintenanceStation_en-US_en-US.pdf (90 Downloads) |
Greetings |
|
Follow us on