7/17/2013 7:31 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, It might be. You should check if all types of HMI panels are supporting there. (most probably it does). There is an info -http://support.automation.siemens.com/WW/view/en/67797516 SIMATIC WinCC Runtime Professional 12 is based on advanced development of WinCC Runtime V7.0 SIMATIC WinCC Runtime Advanced12 is based on a further development of WinCC flexible Runtime 2008 and additionally includes OPC DA Server. Best regards, Hristo Mihalev |
7/17/2013 7:59 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello Ashish, Please refer following details from Manual. WinCC (TIA Portal) is an engineering software for configuring SIMATIC Panels, SIMATIC Industrial PCs, and Standard PCs with the WinCC Runtime Advanced or the SCADA System WinCC Runtime Professional visualization software. WinCC (TIA Portal) is available in four editions, depending on the configurable operator control systems:
With WinCC (TIA Portal), it is also possible to configure a SINUMERIK PC with WinCC Runtime Advanced or WinCC Runtime Professional and HMI devices with SINUMERIK HMI Pro sl RT or SINUMERIK Operate WinCC RT Basic. For more details refer this manual, page no 30. WinCC Professional V12.0 Hope this helps. |
Last edited by: Amit_86 at: 7/17/2013 8:01 AMVANDE MATARAM..... |
|
This contribution was helpful to2 thankful Users |
6/15/2015 1:16 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
|
Follow us on