6/13/2015 11:44 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, On what port of the S5-PLC is the system connected? On the CPU port? What you will need to know is the used protocol (= kind of communication language) the S5 and PC were using. Let us make some guesses. If the PC was directly connected to the CPU port, the protocol is SINEC L1 like, If there is a serial communication board, But you will have to find out the correct protocol anyway (i make a guess on P3964 + RK512). |
Best regards |
|
Follow us on