6/22/2015 6:11 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Tekabi, P0700 = 6 and P1000 = 6 ? |
6/22/2015 6:19 PM | |
Joined: 2/8/2015 Last visit: 7/10/2024 Posts: 462 Rating: (9) |
Hello Constantin, The parameters are set as following: P700=6 P1000=2 P1080=10 P1082=10 P1120=10 P1121=10 P3=3 P918=3 Please look the project and tell me the problems. Thanks for your help AttachmentMM420_PROFIBUS_Controlling.rar (193 Downloads) |
6/22/2015 8:20 PM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012) |
Hi,
can you also upload the MM420 Drive configuration ?
Christoph |
6/23/2015 2:23 AM | |
Joined: 2/8/2015 Last visit: 7/10/2024 Posts: 462 Rating: (9) |
Hi, The MM420 drive configuration is include the file i uploaded. And the project is made by TIA Portal V13 Thanks |
Follow us on