3/2/2013 11:38 AM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Hello, i wish to communicate the following printer with Siemens PLC which one hardware is compatible for this, data will be send in decimal character format from plc to printer like 0000000001 dd "/" mm "/" y "HH / MM / SS and mass 14.75kg etc. http://www.videojet.com/usa/videojet-2300-line-large-character-ink-jet-system Above printer have following External Data Communications Protocol. (see attached) RS-232 point-to-point communications Ethernet 10/100 Base TX network communications I want to send Command Code JDU, PRN, SLA, CAF in character format to third party printer slave device can i use CP343-1 6ES7341-1AH02-0AE0..??? Thanks AttachmentD:\tmp\upload\manual.zip (975 Downloads) |
Last edited by: CS Moderator at: 3/10/2013 4:33 PMattachment reattached Last edited by: Sarfraz Bhatti at: 3/4/2013 12:44 PMMS |
|
7/11/2013 6:26 AM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Sample available here for TIA Portal: Sample program (standard blocks CP 340 / CP 341) zXX21_01_PtP_Com_CP34x.zip for TIA Portal V 11.0 + SP 2
|
7/11/2013 8:49 AM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Dear GILCLEBSON ARAUJO Thanks for message, we will use the http://www.markem-imaje.com/products/case-coding/large-character-valvejet/4020 this is better in comparison of Video Jet. http://www.videojet.com/usa/videojet-2300-line-large-character-ink-jet-system for CP communication following Sample program may help you. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=59577545&caller=view |
MS |
|
8/11/2013 4:32 AM | |
Posts: 1 Rating: (0) |
Hi Sarfraz, Do you have the RS232 communication protocol of Videojet Printer?Can you send to me?
Thank you! |
6/26/2015 8:54 AM | |
Posts: 1 Rating: (0) |
Hi Sarfraz, Do you have the RS232 communication protocol of Videojet Printer?Can you send to me?
Thank you! |
Follow us on