6/26/2015 4:38 PM | |
Posts: 45 Rating: (1) |
I can not access the server logo 0BA8 from other machines (pc) network I have two machines (pc1 and pc2) and a logo 0BA8 I networked both pc and logo using a switch (model: WRT54GL) in one of the pc (pc1), I installed Logosoft V7.0 (with the license key) then I did the upgrade to V7.0 V8 successfully. And in other PC (pc2) I have nothing installed. I have configured the following addresses: logo IP: 192.168.1.3 logo mask: 255.255.255.0 the two PCs on automatic addressing. In Logosoft I enabled remote access control with the pass word "gmt" now with pc1 or pc2 I access the server without problem (password "gmt" image3 see attached file) but the content of the logo Scoreboard does not appear on pc1 pc2 like: see attached file (image1,2) what will I do? please help me Attachmentfichier.docx (150 Downloads) |
6/27/2015 11:14 AM | |
Posts: 45 Rating: (1) |
thank you but I can not find the path of its parameters |
6/27/2015 3:45 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32891 Rating: (4066) |
Look at attachment. |
This contribution was helpful to1 thankful Users |
6/29/2015 8:46 AM | |
Posts: 45 Rating: (1) |
thank you I'll try and answer |
Follow us on