7/8/2015 5:53 AM | |
Posts: 4 Rating: (0) |
Hi, Since 4 July I have a big problem. Suddenly CPU all led's flashing. At boot, no matter if switch is on RUN or STOP, no matter if Flash card is in or not, the initial check fail, the INTF light on steady and all other led's start blinking. I have replace the CPU, able to work with the new one for 30 minutes and then again same think happen, also this CPU started to ALL LEDS BLINKING. I have then try to: My Hardware configuration; No communication with CPU then no diagnostic, totally blind. This are two new CPU. we just start up from few days and we are already at stall.
Closed cause question posted twice. AttachmentCPU 414 all leds blinking.zip (304 Downloads) |
Last edited by: Min_Moderator at: 7/8/2015 9:17:32 AMNew subject after splitting and closed Last edited by: Strafo at: 7/8/2015 1:43:02 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on