7/19/2015 12:54 PM | |
Posts: 52 Rating: (1) |
Hello All Currently i am having PCS7 Project in 8.0 Update 1(Asia) version. Currentlu i am having only one Server. now i have to Add another redundant server with Latest version that is PCS7 V8.0 SP2 Asia version. Project Migration Completed secessfully. After Adding redundant server, complie OS backup without errors. i have downloaded my project on master server secssfully but i am facing problem in redudant server. in the Project path Redudant servers data base was not created after compilation. in downloading following error i am facing . i have attached one rar file.please download file. Thank you all AttachmentServer_Errors.rar (76 Downloads) |
7/20/2015 8:29 AM | |
Posts: 567 Rating: (107) |
Hello,
please check the FAQs "Which settings should you check if OS loading fails with PCS 7 or the OS project cannot be activated?" and "How can you clear the error message "Download (310:88)"?".
|
Follow us on