7/21/2015 1:26 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello guys, Today I had a problem with a client (PCS7 8.0 SP2). The client was restarted and during Wincc explorer it came up with a warning: Database invalid. After that, project could not be opened, could not be downloaded etc. After a while, I saw that the Wincc database of the client was in "single user" mode, instead of multi user mode. The logfile sql server 2008 states: Setting database option SINGLE_USER to ON for database CC_xxxxx. After that, the logfile states: SQL server is terminating. What problem can cause the Wincc database to be set to single user? I now that recently a user was changed (password) in Windows, but nothing else happened. I could set it to multi user again, after that I deleted the client project, downloaded and everything was normal again. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on