7/23/2015 1:48 PM | |
Posts: 9 Rating: (0) |
Hi, This also another attachment please.... AttachmentLEC-OM026xxim_OperatingManual.pdf (402 Downloads) |
7/23/2015 1:50 PM | |
Posts: 5225 Rating: (1185) |
An add on card can be an option.. see attachment. AttachmentExtract_S7-1200 System manual.pdf (450 Downloads) |
7/29/2015 11:31 AM | |
Posts: 9 Rating: (0) |
Hi, How i can get Sink PTO in the CPU 1214C module. Pls let me know |
7/29/2015 11:54 AM | |
Joined: 12/16/2012 Last visit: 4/22/2024 Posts: 652 Rating: (130) |
Hi! One solution would be to use high speed optocouplers between the PLC and the drive. E.g. like this one (100kHz): https://www.phoenixcontact.com/online/portal/us?urile=pxc-oc-itemdetail:pid=2902970 Or a converter: (however, this may be too slow for you at 15kHz) https://www.phoenixcontact.com/online/portal/us?uri=pxc-oc-itemdetail:pid=2964319&library=usen&tab=1 P.S. as I mentioned before, if you have fixed positions, you can use a position table in the drive and normal DO at the PLC - then there's no need for PTO and source to sink interface. |
Last edited by: Kahl at: 7/29/2015 12:03:26 PMadded second link |
|
Follow us on