8/3/2015 7:26 PM | |
Joined: 8/25/2006 Last visit: 9/18/2024 Posts: 2209 Rating: (278)
|
Hello. Communication via CP51M1 also possible as via CP5100. The configuration is the same. There is no difference what type of blocks to use CRV/CTV or CRV_P/CTV_P. Look also at this thread. Regarding occupied port number: try to find all CRV/CTV and CRV_P/CTV_P in the program and check whether they use this port or not. When you configure connection use different local/remote port numbers for each direction. |
This contribution was helpful to1 thankful Users |
8/12/2015 10:51 AM | |
Joined: 8/25/2006 Last visit: 9/18/2024 Posts: 2209 Rating: (278)
|
Yes, I meant uncheck 'Active connection establishment'. |
This contribution was helpful to1 thankful Users |
Follow us on