3/26/2012 1:35 PM | |
Posts: 10 Rating: (0) |
Hello everybody I have achieved a communication between "Logo! 0BA7" and "PC Access", as you can see at the attached files.I am wondering if is it possible to replace "PC Access" with "Simatic Net". What I want to do is to create a Wincc application that must support communication with 50 "Logo 0BA7". The communication will be between PC and every Logo! Separately(each Logo! will have just one connection), that means that the 50 Logo! will not have communication between each other(50 Logo! --> 50 Connections with the PC). Thank you in advance!!!
AttachmentSAMPLE PCACCESS-LOGO!0BA7.zip (947 Downloads) |
Last edited by: Fotis at: 3/26/2012 1:56 PMLast edited by: Fotis at: 3/26/2012 1:36 PM |
|
3/27/2012 7:17 AM | |
Joined: 3/21/2006 Last visit: 3/26/2024 Posts: 10228 Rating: (1180) |
Hello, I am assuming that is possible to use Simatic Net OPC (http://support.automation.siemens.com/WW/view/en/14587200) too. Just take a check which version of SIMATIC WinCC is released for which version of SIMATIC NET and which version of SIMATIC NET is supplied with SIMATIC WinCC is given in Entry ID: 21927773 . Instead of LOGO! assign S7-200 (like in How can you set up a connection between a LOGO! 0BA7 and an HMI Panel? ). And you need to have a extra license (SimaticNet) in order to supports more then 8 connections... Try it...But If the trick is much cheaper using PC Access... Best regards, Hristo Mihalev |
3/29/2012 3:06 PM | |
Posts: 2930 Rating: (432)
|
Hi, there is no trick just add your 42 IP addresses to PC Access. The first chanel will be used automatically. Nothing necessary. regards |
7/24/2015 10:58 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4777 Rating: (123) |
|
8/12/2015 2:30 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4777 Rating: (123) |
New question published by davidwill is split to a separate thread with the subject Siemans Logo 0BA8 to a Weintek MT8050ie HMI. Best regards |
Follow us on