7/28/2015 12:28 PM | |
Joined: 7/29/2014 Last visit: 9/4/2024 Posts: 43 Rating: (3) |
Edit after moved from CFC changes topic:
Had the same CFC undo problem with the same 7.0SP1 version, basically what I worked on yesterday was gone today. Killer frustration... Just searching for the hotfix you mentioned, by the way available at https://support.industry.siemens.com/cs/document/41729780/hotfix-8-for-cfc-v7.0-sp1?dti=0&dl=en&lc=de-WW is not exactly straightforward.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/28/2015 4:17:29 PMNew subject after splitting Last edited by: norenendur at: 7/28/2015 5:57:35 PM |
|
7/30/2015 7:51 AM | |
Joined: 7/29/2014 Last visit: 9/4/2024 Posts: 43 Rating: (3) |
Guess not. Will Google each and every package... |
8/6/2015 4:35 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating: (40)
|
norenendur, I recommend two things... 1- Archive often (when programming, at least at the end of each day). This will make sure that what you work on today is never lost. 2- If you are looking for what is released for your PCS 7 version, you can consult the PCS 7 Compatibility Matrix for your version of PCS 7. You can get to them here, http://www.siemens.com/kompatool I do the 'download lists' and select the version I want, in your case, select V7.0 and the spreadsheet will show all releases for each service pack within V7.0. Thus if you need a certain release, you may need to consider upgrading. Goodluck! |
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
Follow us on