8/20/2015 6:26 PM | |
Joined: 11/29/2011 Last visit: 8/19/2024 Posts: 1359 Rating: (232) |
Hi, If you upload the OS compilation log it is easier to comment on. In the OS compilation dialogue there is a tick box called "Picture Tree". Keep that in mind. Maybe have a look at SIMATIC Process Control System PCS 7 Compendium Part A - Configuration Guidelines (V8.1) page 229, where you can read: "The picture hierarchy (Picture Tree) is automatically generated during OS compilation in accordance with the plant hierarchy settings in the SIMATIC Manager." So if you had custom built Picture Tree that can be the cause. Upload the compilation log so we can have a closer look. I hope I could help! |
Last edited by: MicroMan at: 8/20/2015 9:03:52 PM- What you read here, please check with manuals and your requirements. |
|
8/21/2015 10:25 AM | |
Joined: 11/30/2011 Last visit: 7/15/2024 Posts: 31 Rating: (1) |
Dear MicroMan, Thanks for your suggestion, I have tried your solution but problem is still there. A strange thing happen, i change CPU410-5H Version 8.0 to 8.1 in hardware configuration of my project and problem solved. I don't understand why PCS7 behave like this. |
Follow us on