8/24/2015 11:20 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi, here is a basic instruction for communicating with the reader via RF120C communication module: Configure your HW: Insert the blocks you need: Create your connection DB: Call your blocks in OB1 or another FB (which is called in an OB): Check out this documentation for more info on the ident instructions:
I hope this helps a little bit. If you have further questions don't hesitate to ask. |
Last edited by: Owei at: 8/24/2015 11:25:07 AMLast edited by: Owei at: 8/24/2015 11:27:22 AMLast edited by: Owei at: 8/24/2015 11:27:38 AMLast edited by: Owei at: 8/24/2015 11:28:31 AM |
|
This contribution was helpful to1 thankful Users |
8/28/2015 8:53 AM | |
Joined: 10/28/2014 Last visit: 9/24/2024 Posts: 3 Rating: (1) |
Hi , Its really simple to configure first just configure the right GSD file with right firmwire , use Mobby DB to configure , here is the attachment i have given, Once you configure and download the reader will show yellow light blinking then it will turn from red to green , use fb 45, here is the link it will help https://support.industry.siemens.com/cs/de/en/view/88779859,You will get lot of examples with 300 PLC migrate it and it will certainly works , need assistance you can contact me Command B#16#2 Sub Command B#16#0 Length 8 Address_MDS W#16#FFF0 DAT_DB number 48 DAT_DB address 0 My DAT_DB 48 is ot type byte up to 1024. bye Regards Shiva Giragani
AttachmentMOBY_DB.pdf (362 Downloads) |
Follow us on