9/1/2015 3:49 PM | |
Posts: 5 Rating: (0) |
Dear Experts , I am working at a cement factory and i have a problem with a micromaster 440 , 200kW This converter drives a induction motor 160kW installed on a dynamic separator application. The converter is stopping many times from alarm A0911 . On the converter is installed an braking unit type 6SE7028-0EA87-2DA0 and a resistor 50kW . P1120=150 P1121=290 Please suggest smth to eliminate this alarm . ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/2/2015 11:25:56 AMNew subject after splitting |
|
9/2/2015 11:27 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on