9/2/2015 9:36 AM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
Dear see attached plc ladder file. can u tell me where it calls G54 plc program routine because when i apply G54 command only Z axis will not move in JOG mode but all other axis are working fine in JOG mode. listen this is new machine and on startup phase so may be there is plc program issue. so if i find where the G54 command routine in plc then i can see why only z axis is not working in JOG mode. all inputs of JOG key are fine and ok. AttachmentPLC Ladder.pdf (188 Downloads) |
Muhammad Munir |
|
Follow us on