3/2/2015 12:37 PM | |
Joined: 1/17/2007 Last visit: 4/19/2024 Posts: 69 Rating: (0) |
I have in mind that in the past it was possible to export/import tags from WinCC pdl picture, a way similar to export / import teksts from a picture. And this is not a PCS7 tools for objects. But I am not sure if I am remembering right, since I cannot find it. Can you help me if somewhere exists a tool for this. The functionality for linking (which is inside Graphic Designer) is not an option, since at the beggining all tags will be the same, so I can not replace tags using this tool. My reference is object name and thats why I need to export picture object and put for every object a tag regarding it's name. Edit: Need a tool for searching & replacing tags/text and so in Siemens' WinCC PDL files. |
Last edited by: Jura at: 3/2/2015 12:41:51 PMLast edited by: Jura at: 3/2/2015 12:42:54 PMLast edited by: Jura at: 3/2/2015 12:50:05 PM |
|
3/2/2015 1:38 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Jura, I think, you speak about the Tool "Easy Language". It was need before WinCC V7. Since V7, WinCC has the TextDistributor. For "Easy Language". see https://support.industry.siemens.com/cs/ww/en/view/29419870 For ASIA-Version the Tool "TextPort" was used (here would you need MS Access), see: https://support.industry.siemens.com/cs/ww/en/view/22449303 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
9/7/2015 3:31 PM | |
Posts: 1 Rating: (0) |
Hi Jura Are you maybe looking for the Dynamic wizard ? It has a Import / Export and a update picture objects wizard that can possibly do what u require. |
Follow us on