9/15/2015 11:18 AM | |
Joined: 5/1/2013 Last visit: 3/29/2024 Posts: 426 Rating: (3) |
텍스트 또는 웹사이트 주소를 입력하거나 문서를 번역하세요. naega deulaibeu dp setinghal ttae, naega peuloseseu imiji seoljeong-eul haji anh-eumyeon, eotteon munjega balsaeng hal su issneunga? 이것을 찾으셨나요? 드라이브에 세팅할 When I drive dp setting, if I do not set a process image, is there any problem can occur? Attachmentsetting.pdf (97 Downloads) |
9/15/2015 2:47 PM | |
Joined: 6/24/2013 Last visit: 4/22/2024 Posts: 1588 Rating: (409) |
Hi You can switch process image OFF and just copy the data to/from drive using move instruction or SFC. for example for 6 words from 760 L PID760 // 760 to 763 t LD0 L PID764 // 764 to 767 t LD4 L PID768 // 768 to 771 t LD8 outputs (assume 6 output words from 760)<FILL IN OUTPUTS BEFORE COPYING> L LD12 T PQD760 // 760 to 763 L LD16 T PQD764 // 764 to 767 L LD20 T PQD768 // 768 to 771 in the above example you have your drive data in local variables: L0.0 to L11.7 for inputs (6words) L12.0 to L23.7 for outputs (6 words) This way You can access them in anyway (for example status word bit-by-bit; int speed setpoint as integer; etc.) Also note that bits in status word are swapped example of drive block (for GU120 drive) attached. AttachmentFC19_GU120_drive.pdf (80 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on