9/17/2015 5:59 AM | |
Posts: 3 Rating: (0) |
Hello, I request an English language version of the following two documents: (a) https://cache.industry.siemens.com/dl/files/932/8790932/att_82256/v1/norm_tab.pdf (b) https://cache.industry.siemens.com/dl/files/748/109476748/att_845617/v1/IEC_61131_compliance_de_DE.pdf Further, I request further information (in English) on the subject of: (a) why Step 7 is not in full compliance with IEC 61131-3: 2013 (see Tables 48 to 53 in this standard) and (b) what is Siemen's policy is towards full compliance with IEC 61131-3: 2013. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 9/17/2015 11:57:21 AMNew subject after splitting |
|
9/17/2015 7:10 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello, I request an English language version of the following two documents: (a) https://cache.industry.siemens.com/dl/files/932/8790932/att_82256/v1/norm_tab.pdf (b) https://cache.industry.siemens.com/dl/files/748/109476748/att_845617/v1/IEC_61131_compliance_de_DE.pdf I think you are looking for the following links in English: General Product Approval, Manufacturer declartion, ManufacturerI hope this helps, hdhosseini |
9/17/2015 7:34 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello More Details ( Including the English Version of the document that you are referring to ) are available in this FAQ : https://support.industry.siemens.com/cs/in/en/view/50204938 Some more information here : Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
9/18/2015 2:31 AM | |
Posts: 3 Rating: (0) |
Dear Sirs, Why have Siemens not implemented the object orientated features of Tables 48 to 53 in IEC 61131-3: 2013? The table titles are:
I would have thought that these tables constitute the fundamental changes in the Standard from the 2nd (2003) to the 3rd (2013) Edition? Would somebody suggest to whom in Siemens this matter may be addressed to, should my query be outside the scope of the Support forum? Thanks eamonnatwork
|
Follow us on