10/1/2015 9:16 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446) |
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
By clicking on button a Report is sent to the printer.
Requirements: WinCC V7.3.
Project with a minimum configuration (stop button, tags, etc.).
At least one printer driver installed and set as default printer in Windows.
Configuration main steps:
#include "apdefap.h" void OnClick(char* lpszPictureName, char* lpszObjectName, char* lpszPropertyName) { // WINCC:TAGNAME_SECTION_START // syntax: #define TagNameInAction "DMTagName" // next TagID : 1 // WINCC:TAGNAME_SECTION_END
// WINCC:PICNAME_SECTION_START // syntax: #define PicNameInAction "PictureName" // next PicID : 1 // WINCC:PICNAME_SECTION_END RPTJobPrint( "Print Job 001" ); //Return-Type: BOOL
}
Note: is not possible, at actual state of art, to start a print job directly by VB script. Alternative – add a Print job diagnose object (just for diagnose proposes) Place a Application Windows (Smart Objects) Configure the Application Windows (Windows contents → Print Jobs → All Jobs). Thanks to the Siemens United States Technical Support (in special Mr. David Crockett) for the Help with this TIP.
References: Portal SIMATIC WinCC in Online Support https://support.industry.siemens.com/cs/br/pt/view/93906404/en
Manual WinCC V7.3: Working with WinCC https://support.industry.siemens.com/cs/ww/en/view/102754925
WinCC V7.3 Scripting: VBS, ANSI-C, VBA https://support.industry.siemens.com/cs/ww/en/view/102777678
Application and tools Demo projects for SIMATIC WinCC V7.3 https://support.industry.siemens.com/cs/br/pt/view/93148272/en
Example Blocks for WinCC V7 and STEP 7 V5 (for S7-300 with SCL and S7-400 with CFC, SCL) https://support.industry.siemens.com/cs/br/pt/view/68679830/en
Example blocks for WinCC V7 and STEP 7 (TIA Portal) (for S7-1200 and S7-1500 in SCL) https://support.industry.siemens.com/cs/br/pt/view/31624179/en
Project: Due a size / format restrictions, the project are first compacted with 7z format (project.z7) and after that attached to a zip archive (data.zip). Attachmentdata.zip (794 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to6 thankful Users |
Follow us on