10/8/2015 7:57 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
In this simple sample, points are plotted on trend view object by button click (the concept could be extended to controller commands).
There are two variants: On demand, where the plotting is done by change bit variable and cyclic selective, where the plotting is enable / disable para bit state.
Requirements: WinCC Professional V13 SP1.
Project with a minimum configuration (stop button, tags, etc.).
Configuration main steps:
On demand
Cyclic Selective
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Project: Project attached as project.zip
AttachmentProject.zip (239 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |
Follow us on