8/25/2015 11:09 AM | |
Posts: 8 Rating: (0) |
Hello guys, I need some help! I have 1 inverter (MM430) communication with S7-200 (CPU 224XP) via the USS protocol. However, I can only control inverter start / stop and change the frequency but can not read parameters from the inverter (such as current, status,...). I get error codes 01 (drive did not respond). My program test in attachments Thank you very much! Attachmenttest.pdf (384 Downloads) |
10/22/2015 10:57 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by luis2 is split to a separate thread with the subject Communicate a s7-200 with my laptop. Best regards |
Follow us on