10/24/2015 1:01 PM | |
Joined: 12/7/2011 Last visit: 8/16/2024 Posts: 384 Rating: (9) |
Hi to all. I would ask your support about the Step7 Online HW Diagnostic. i have a project with Three Profibus DP networks. The first one is connected on the CPU, and are connected some Siemens Protections. The second and third one are connected each on one CP 342-5, and on it are connected some MCC slot for each one. When from the Step7 i select the Online HW Diagnostic, i see in the first line (CPU line) which device is ok or not (through the red line). On the second and third i see always the device's icon matt, and the only way to see if are ok or not, is open the CPs specific diagnostic. Anyone knows if it's normal or not? Thanks. Regards Alfredo Attachmentspecific diagnostic.pdf (105 Downloads) |
Last edited by: Alfredo@as99 at: 10/24/2015 1:04:40 PM |
|
Follow us on