10/27/2015 9:31 PM | |
Posts: 111 Rating: (1) |
I want to activate the motor through remote I/O's so will I be able to directly actuate the coil of contactor from the output card (6ES7132-6BH00-0BA0) or do I have to use a relay before the coil of the motor. Can anybody tell? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/28/2015 2:33:50 PMNew subject after splitting |
|
10/29/2015 1:01 PM | |
Joined: 5/28/2008 Last visit: 4/26/2024 Posts: 1343 Rating: (141) |
As you can see in the technical data, you are able to switch loads with 0.5A. https://support.industry.siemens.com/cs/de/en/pv/6ES7132-6BH00-0BA0/td
For direct switching a motor, I would prefer to take a relay in between.
|
11/2/2015 10:16 AM | |
Posts: 38 Rating: (0) |
It's not a good idea to directly switch a motor, always use a contactor. |
Follow us on