11/3/2015 3:46 PM | |
Joined: 12/18/2014 Last visit: 3/28/2024 Posts: 32630 Rating: (4044) |
Look at attachment. |
11/3/2015 3:55 PM | |
Joined: 8/5/2015 Last visit: 9/20/2021 Posts: 120 Rating: (3) |
i try it of 4 mA i get 0 % but in 6mA i have 100 |
11/3/2015 5:25 PM | |
Joined: 12/27/2006 Last visit: 3/23/2024 Posts: 1195 Rating: (112) |
Let us show what parameters you have set in the analog block. Post your programm, and we can see whats going wrong. |
11/3/2015 6:29 PM | |
Joined: 12/18/2014 Last visit: 3/28/2024 Posts: 32630 Rating: (4044) |
Here is the file, for example.
AttachmentSchaltplan1.zip (155 Downloads) |
11/4/2015 7:32 AM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating: (0) |
is the value whne you inject 6mA maximum? |
11/4/2015 4:37 PM | |
Joined: 12/18/2014 Last visit: 3/28/2024 Posts: 32630 Rating: (4044) |
Here's a little more Information.
AttachmentLogo overview analog voltage current units.pdf (184 Downloads) |
Follow us on