11/19/2009 3:33 AM | |
Posts: 262 Rating: (45) |
HiGurise, 2) Energy use cant be displayed.. Please appreciate that it is a Configuration Software for PAC meters, however for trendz etc you require some energy monitoring software like SENTRON POWER MANAGER.Or else if, you have WINCC / PCS 7 based SCADA system from Siemens than can use a Add On software called Power Rate where you can see all the Graphical representation etc.The below URL can be used to see some demo:- www.siemens.de/powermanagementsystem |
Last edited by: Valli at: 3/19/2010 9:40 AM |
|
This contribution was helpful to1 thankful Users |
1/28/2011 12:24 PM | |
Posts: 50 Rating: (6)
|
Hello, The SENTRON powerconfig software can´t be downloaded directly from the Siemens Service & Support portal. To acquire the software you need to contact the Siemens Technical Support first. They will provide the softwareon a download server. Sorry but that isthe only option. Here you can find the contact detail of the SiemensTechnical Support Look to My Support -> Support Request http://support.automation.siemens.com/WW/view/en/43500476/133200 |
Follow us on