2/10/2012 4:55 PM | |
Posts: 7 Rating: (1) |
Hello balachandar Configure a drive in PROFINET is quite easy; basically you have to assign the IP address, assign the name and choose the telegram. Also you have to configure the same telegram in the drive in P0922 P0922 - Selects the PROFIdrive Standard Telegram. Value: 1: Standard Telegram 1 20: Standard Telegram 20 350: Standard Telegram 350 352: Standard Telegram 352 353: Standard Telegram 353 354: Standard Telegram 354 Attached is an excerpt of how to configure the drive. You can see also al example: SINAMICS G120 with CU240S PN (FW3.2): Control via PROFINET http://support.automation.siemens.com/WW/view/en/45287261 I hope this help!!! AFP AttachmentS7-300 - PROFINET - CU240S-PN.pdf (769 Downloads) |
11/16/2015 1:35 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by S P Aghera is split to a separate thread with the subject Connect Sinamics G120 VFD ( CU 240 ) with PC. Best regards |
Follow us on