12/1/2015 8:26 AM | |
Joined: 6/14/2006 Last visit: 4/29/2024 Posts: 301 Rating: (60) |
Hi Thunderstorm, as mark said there is the PCS 7 Industry Library that gives a quite easy way for the integration of S7-300 package units into a PCS 7 project. Up to now there is nothing similar for S7-1500 available. So at the moment if there is a need to integrate a small package unit into PCS 7 I would go with S7-300. More info can be found here: https://support.industry.siemens.com/cs/ww/de/view/50708061 Regards |
This contribution was helpful to1 thankful Users |
12/1/2015 5:58 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
I think, it is difficult to convince the supplier to change the controller. Mostly, the have their basic concept and planning. It is right, that you have to do the engineering of S7-1200 and S7-1500 in the TIA Portal. You can connect the S7-1200 / S7-1500 via OpenPCS 7 or PCS 7/OPEN OS
PCS 7/OPEN OS OpenPCS 7 Industry Library
|
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to2 thankful Users |
Follow us on