1/16/2012 10:22 AM | |
Posts: 9 Rating: (0) |
We have installed SP2 HF 6 and this appears to have resolved the problem. |
This contribution was helpful to1 thankful Users |
5/14/2014 7:57 PM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
[quote user="DanielOnline"]You have chance because I have exactly the same problem with Project Duplicator. But I work with Version WinCC V7.0 SP3 Upd 6 !!! Daniel In a redundant environment, Project Duplicator with a running project should work but in the past we failed to get it working and stable. Therefor, we switch to use an ES (with NCM Manager or Simatic Manager), using this we don't need to duplicate manually anymore. Download changes/full download from ES does it all. |
B r g d s , |
|
12/10/2015 3:35 PM | |
Posts: 7 Rating: (0) |
Dear Wizards, I am also facing the problems in duplicating project from server 1 to server 2, At end I am getting message as attached. I am also attaching the procedure of wincc project duplicate. With same procedure, another set of server's the project duplication are sucessful Required tips to resolve the issue. thanks in advance. regards AttachmentWincc project duplication procedure.zip (566 Downloads) |
Follow us on