12/16/2015 8:26 AM | |
Posts: 45 Rating: (1) |
Dear experts, I have a server-client project NOT Redundant that i update from v7.0 to v.7.3. The project is : 1. Server Windows Server 2008, Step7 v5.5 SP4, WinCC v7.0+SP2+UP7 2. Server Windows Server 2012 R2, WinCC v7.3+UP7 (NEW Server) 3. Client Windows 7 SP1, WinCC v7.0+SP2+UP7 4. Client Windows 7 SP1, WinCC v7.3+UP7(Previously WinCC v7.0+SP2+UP7) In order not to leave the client without SCADA we proceed to the upgrade of one pair server-client and after we finish we will update the second pair. After updating the client to v7.3 when wincc starter i was getting the massage "Start picture not found" and whatever picture i was choosing from the popup dialog i was getting the same massage. Even if was choosing the same start screen as the server. My start screen on server is @SCREEN.pdl. Attached screens Start picture, Start Screen selection and Start Screen selection1. Sorry for the bad resolution. I manage to solve this problem by creating same user/passwords for Windows login and WinCC. Although the second pair that is not upgraded yet have different user/pass for windows login. Now the new problem that i have on upgraded client is that WinCC starts normally but the only available functions on start screen is "Acknowledge Button" and "User/password" field. Please see attached picture Grey Areas I want to fix this problem before proceeding with the upgrade of second pair of server-client, so any help will be appreciated Thanks in advance
AttachmentWTE-Mia Millia.rar (184 Downloads) |
Follow us on