Industry Online Support
Technical Forum
2/15/2008 12:43 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi Zoran, in your configuration you can use the MC45 only for SMS Sending/receiving. Maybe check therefore the configuration hier http://support.automation.siemens.com/WW/view/en/25545680 But there is no posibillity for using teleservice. Therefore you need a teleserviceadapter directly connected to the MPI interface of your S7-3xx controller! No teleservice possible through the CP3xx. What do you want? SMS or Teleservice? regards |
2/15/2008 2:43 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi again, ok then a simple answer here: SMS solution with your hardware equipment: http://support.automation.siemens.com/WW/view/en/25545680 Maybe the MC35i differs a little bit from the MD720-3 regarding the AT-commands and the behavior of reaction. In this case you have to adjust the program. GPRS solution with your hardware equipment: there is now already existing solution for that. Why not change MC45i to MD720-3? There will be solution available in march 2008. regards AttachmentAT_Command_Set_MD720-3.zip (590 Downloads) |
2/15/2008 4:23 PM | |
Joined: 1/25/2006 Last visit: 7/27/2024 Posts: 257 Rating: (60) |
Thank you, Lifrasil, for your help. B. regards, Zoran |
Follow us on