12/29/2015 1:12 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hello, Because you need a TTY communication which is not available on a PC (only on the PGs) I recomend a V24 to TTY cable or when you didn't have a V24 (RS232) port then a USB to TTY cable. Why does the online mode not work with the S5-PC converter TTY - RS 232? For a USB/TTY cable you have to serach on Internet for one that is working together with STEP5. Because the power of the TTY have to be coming from the TTY interface of the S5 CPU 090 you have to look very well what you are buying. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on