11/15/2009 4:46 PM | |
Posts: 3 Rating: (0) |
Dear ChristophD, I'm using SINUMERIK 802Dsl pro with Smart line 10 kw (without Drive CLIQ), SINAMICS120 and I also have the same problem like Andrew's: p0009 in CU = 0, p0010 in drive=0. I connected X21 pin 1 of SML to X20 pin 1 on CU. When I click buton "Drive ON" in Control panel in STARTER, ISCOA: 30020: The switch on disable of the drive is active!<!--[endif]--> appear. I can not turn the motor on. Please help me. AttachmentError.pdf (280 Downloads) |
Last edited by: O_Moderator at: 11/16/2009 8:45 AMnew subject after splitting from /tf/WW/en/Posts/25637#top |
|
11/16/2009 8:56 AM | |
Posts: 3 Rating: (0) |
Hi ChristophD The value of the parameter r46 of SERVO_02 is 40001C0F. Value of the paramter p864 of SERVO_02 is set via r722.0 ( connected to "smart line ready" signal). I'm sending you attached file with config and some screenshot, please help me. Thank you very much. AttachmentChristophD.zip (229 Downloads) |
11/18/2009 11:44 AM | |
Posts: 1 Rating: (0) |
Hello! I have same problem like you do...details are in pdf..., I hope so that sombody can help me. You will see that in my system motor works in one way but in the other way i have this famous error "The switch - on disable of the drive is active"... Best regards! Zarac AttachmentCPU310 DP_configuration_zarac.pdf (357 Downloads) |
2/2/2016 3:39 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by alex s120 is split to a separate thread with the subject s110 with CU305, fault 7930. Best regards |
Follow us on