2/5/2016 5:05 PM | |
Joined: 5/27/2014 Last visit: 10/26/2022 Posts: 109 Rating: (6) |
Hi there, I got a few question, maybe I'm doing it totally wrong, so please show me the right way. I'm using Recipes and trying to make button, which change a picture, according if recipe is activated or not. I tried to create faceplate, put on/off pictures in graphic list, but to make this dynamic, so I don't have to create 30 faceplate buttons. So basically, when the faceplate will be done, I need to put number in InterfaceProperties, which will indicate, for which recipe (1,2,3...) will this button be used and change a picture, if recipe is activated or not. Wow too complicated. Another question, can I show name of recipe (IO filed maybe)? I only know, how to show name of active recipe, through tag. [snip] Thanks for any advices TIA V13 SP1, WinCC Advanced V13 SP1, TP700 Comfort ---------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 2/8/2016 10:53:01 AMForum question split TIA V16 update 4, STEP 7 Professional+safety |
|
Follow us on