6/23/2015 8:24 PM | |
Posts: 2 Rating: (0) |
dear experts! I have the same error... but i don't believe it's because the resources on the computer. Where we have the error is on the project tree menu, that was automatically created by "OS project editor", specifically when we change from screen to screen I have a Intel i5 processor and 8gb of ram with windows 7-64bit I recently updated winCC/Webnavigator from V7.3+upd1 to V7.3+upd5 but still having the same error, probably a little less... WebNavigator is compatible according to the tool, with iexplorer v11.0.9 I don't really know how this control-surrogate works. I haven't found anything directly from siemens. this is what I found on other sites; **** The web server or application must be capable of receiving the Surrogate-Capability headers and identifying whether the ID is acceptible. {X} Special care may be needed. The ID tags "unset-id" , "unconfigured" and "localhost", "localhost.localdomain" are known to possibly be sent by many broken or mis-configured proxies. The web server or application then adds a Surrogate-Control header in its HTTP replies containing the instructions which are to be used instead of the Cache-Control header settings. Details about Surrogate-Control can be found at http://www.w3.org/TR/edge-arch **** But i have not clue where or what I can check or move on the configuration for WebNavigator I hope you can help!! thanks!! ----------------------------------------------------------------------------------------------------
Split from Control Surrogate Error in Web Navigator. |
Last edited by: Min_Moderator at: 6/24/2015 12:49:41 PMNew subject after splitting |
|
2/17/2016 3:46 AM | |
Posts: 1 Rating: (0) |
amaldonado, I am having the same error. It has been 7 months since this post. What have you done to fix this? Or has it remained an ongoing issue? |
Follow us on