Industry Online Support
Technical Forum
2/29/2008 9:49 AM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hi ntban, -------------------------------------------- (1) access database in vb -------------------------------------------- http://www.vbexplorer.com/VBExplorer/vb_feature/june2000/Database_Beginner_ADO_DAO.asp -------------------------------------------- (2) enable/disable keys -------------------------------------------- there is allways a windows user logged on, when´wincc is in runtime mode!!!! In the dialog "Computer properties > Parameter" of wincc control center you can find chekboxes to enable/disable special windows hotkeys (Ctrl+Alt+Del, Alt+Tab, Ctrl+Esc, Alt+Esc) ==> this configuration do not allow the current user. But it is possible to enable/disable the windows hotkeys dependingon the current user (wincc logon) http://support.automation.siemens.com/WW/view/en/27068495 |
3/1/2008 1:14 AM | |
Joined: 11/9/2007 Last visit: 4/8/2023 Posts: 25 Rating: (0) |
Hello i have same problem.I want write some tags for exp TAG1,TAG2 in "Proces_Table" TAG1 and TAG2 column at sql database every ten second.First where am i write this script in wincc ?(VBS-editor /actions or Standart modul or project module) thank you for your inform |
Follow us on