5/10/2010 11:08 AM | |
Posts: 267 Rating: (24) |
Hello! here is a sample to send the string from the S7-1200 to HyperTerminal. You need a null modem cable (http://www.nullmodem.com/NullModem.htm)to connect the CM1241 to the serial RS232 port of your PC. The port settings for the CM1241 (in the HW configuration) and for HyperTerminal are the default ones. It works! But I don't know, where the note comes from! AttachmentRS232.zip (4439 Downloads) |
This contribution was helpful to1 thankful Users |
5/16/2010 12:06 AM | |
Posts: 5 Rating: (0) |
Hello! I do not understand how it works TAG "0_5Hz" on REQ input in the SEND_PTP module? Can someone help me understand this? Best regards Andrzej |
5/16/2010 9:11 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello, To enable transmission of data its need a rising edge on this input REQ. So, this tag is continuously pulse. More details at SIMATIC STEP 7 Basic V10.5 from 987 page. Perhaps also there have some useful info for future http://support.automation.siemens.com/WW/view/en/42002283 Best regards, Hristo Mihalev |
5/16/2010 8:02 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello, Look at How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? I think this FAQ will clarify situation. Best regards, Hristo Mihalev |
5/26/2015 11:27 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
9/3/2015 1:36 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by anil.yadav091 is split to a separate thread with the subject RS-232 in s7-1200. Best regards |
This contribution was helpful to1 thankful Users |
10/28/2015 10:41 PM | |
Joined: 4/3/2012 Last visit: 9/6/2024 Posts: 18 Rating: (1) |
Is there a V13 version of this program example? I can't open V10. |
2/22/2016 10:28 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by mostafafawzy5 is split to a separate thread with the subject How to connect 2 plcs' (1200) via rs 232?. Best regards |
Follow us on