3/15/2016 9:04 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello GREY, Do all charts have the "PH Assignment" when you are in Component view and when clicking on "Charts" folder (with exception of @-charts) and when you do a compile, do you see that an OS assignment was set for your plant hierarchy? If not, you need to make sure that the charts have an AS-OS assignment |
Last edited by: Oreca at: 3/15/2016 9:08:42 AMIf I could help you, you can use the RATE button. Thank you. |
|
3/15/2016 10:05 AM | |
Joined: 11/29/2011 Last visit: 5/7/2024 Posts: 1358 Rating: (230) |
Hi, Check the SIMATIC Process Control System PCS 7 Compendium Part A - Configuration Guidelines (V8.1) on page 75 under "Making PH settings". Maybe the tag are generated but they not include the HID while other tags does. Make sure that all the PH is set up on the same way and life gets simpler. |
- What you read here, please check with manuals and your requirements. |
|
3/15/2016 11:05 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
In addition to Micromans post, if that does not solve the issue: - Did you do a Full compile CFC and Full compile OS with memory reset? If not, please do so - In plant view under your AS project-> right click->Plant hierarchy->Check Consistency. A check is made to see if there are any problems. Report any issues |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/16/2016 4:56 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello GREY, Ah, that is good to hear! I was afraid you needed to create a support request haha. Microman and me like ratings |
If I could help you, you can use the RATE button. Thank you. |
|
3/17/2016 8:13 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello Grey, Thanks! For your next problem: Did you change the interface of a block? If so, you need to update block types first. In CFC, go to Options->Block types and select the block you changed on the left side of the columns and press the "->". The block is now updated to your CFC program/charts. Carefull! The editor can give out three results: Block interface did not change, Block interface did change, but can be downloaded in run, Block interface did change, PLC must go to stop. If you click OK for the last result, you have to download the complete program in stop mode. After your downloaded the block, then you have to do a OS compile. The reason for this error is because the name or attribute of an OS relevant block parameter has been changed. |
Last edited by: Oreca at: 3/17/2016 8:18:48 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on