5/14/2014 3:01 PM | |
Joined: 6/24/2013 Last visit: 5/8/2024 Posts: 1596 Rating: (410) |
Hi Working solution with homing and conversion to eng unit attached. The FC block is the init (call it in OB100). the FB is called in every scan. AttachmentFC203_FB200.pdf (739 Downloads) |
This contribution was helpful to2 thankful Users |
3/21/2016 3:12 PM | |
Posts: 6 Rating: (0) |
Dear Friends I am P. PradeepKumar working in Salem Steel Plant - Salem - Tamil Nadu - India as Automation Engineer . I am using FM350-1 counter Modules in 6 Coin Counting Machines which counts the Blank coins (Indian Rupee) and those counted coins are packed to Mint for Govt impression. Earlier i was using the FM350-1 Module, each per one machine. Thus i needed 6 Modules. Now I replaced all the 6 FM350-1 modules by a single FM 350-2 Module which can even be used for 2 more Machines (Total of 8 Machines) After Installing the CD, we get FC 2,3,4,5 and its respective FBs and DBs from the Library. Copy those into our program. Then call FC2, FC3, FC4 as shown in the attached program. The Batch number of 100 and 101 should be used before calling 'RD FC' to read the Counts contents in Double Word Format(DINT). All the 8 channels are working beautifully in DINT format. Pl see the attached program and use it Pradeepkumar Pl convey your feedback please AttachmentTEST_S7_21032016_6PM_Good.zip (471 Downloads) |
Last edited by: Min_Moderator at: 3/22/2016 2:27:22 PMContact data deleted |
|
3/21/2016 3:38 PM | |
Posts: 6 Rating: (0) |
Hai....Good Morning.... I am Pradeepkumar working in Salem Steel Plant Salem Tamil Nadu India. Pl go thro the attchment program and do modify your program, it will work. After Installing the FM 350-2 Installation CD, Copy the FC 2,3,4,5 and its corresponding FBs and DBs from Library and paste all into your program. Then call them as shown in my program with out forgetting to write the Batch number of 100, 101 before calling the 'RD FC' . I am using this program for my 6 counting machines to count the blank coins in our Coin Blanking Line. I replaced 6 Nos of FM350-1 module by a single FM350-2 Module. Now i can go for 2 more machines as it works for 8 Channels. We can get the DINT format(32bit) count output. Pl go thro the attched program and use it. Tell me your feedback Pradeepkumar AttachmentTEST_S7_21032016_6PM_Good.zip (380 Downloads) |
Last edited by: Min_Moderator at: 3/22/2016 2:27:35 PMContact data deleted |
|
Follow us on