3/29/2016 7:50 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hello Cammo, Unfortunately, you cannot do what you want, however, there are some things that can work: 1. If only one bit is active in the word, you can compare the word with a value like 16#FFFFFE. If more bits are active, then you cannot do this. 2. If your WORD is a structure of bits, then you can address each bit individually like you want. 3. You can use the standard block: W_BO of the family: CONVERT, which has a WORD as input and BO as outputs. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on