4/2/2016 11:25 AM | |
Posts: 142 Rating: (2) |
Piscean bro i have an external encoder which is Delta incremental rotary encoder having code ES3-0CVN6941 |
4/2/2016 12:30 PM | |
Posts: 142 Rating: (2) |
yeah bro piscean but if u have any doubt on parameters then u can ask . |
4/2/2016 12:36 PM | |
Posts: 1529 Rating: (202) |
In STARTER (or in the attached case, SCOUT, but the screens are the same), you should have this encoder configuration screen. |
4/2/2016 12:44 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, With encoder pulses 360, are you facing any problem? This post was started, as how r485 encoder counter values are increasing. To which expert, TechTeam replied. Then you wanted to know how angular position is calculated. To which answer is given. Also I asked you if this problem is related to your another post F0090 Error, which you did not replied. Now you are confused about encoder PPR. What is your exact problem?
|
4/2/2016 1:12 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Ok. Please attach here with complete back up of program. |
Follow us on