4/4/2016 7:13 PM | |
Posts: 2 Rating: (0) |
Hello, I'd like to know if the Y-Couple 6ES7 197-1LB00-0XA0 works with IM 6ES7 153-2BA82-0XB0. Thank you,
|
4/4/2016 10:54 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello Drisao; The 6ES7153-2BA82-0XB0 has been phased-out by Siemens in November 2015, and is now replaced with model 6ES7153-2BA70-0XB0. But if you have 2 numbers 6ES7153-2BA82-0XB0 in your possession, along with a Y-Coupler 6ES7197-1LB00-0XA0 (and the required active bus modules and special mounting rail for bus modules such as the 6ES7195 1GA00 0XA0, l=480 mm). you can build a working Y-Link, without loss of functionality. The following FAQ will give you the hardware requirements for building a Y-Link, including "predecessor products": How is the Y link structured? https://support.industry.siemens.com/cs/ww/en/view/43688632 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/4/2016 10:55:55 PMLast edited by: dchartier at: 4/4/2016 10:56:35 PM |
|
This contribution was helpful to1 thankful Users |
4/5/2016 5:31 PM | |
Posts: 2 Rating: (0) |
Thank you very much |
Follow us on