Industry Online Support
Technical Forum
4/13/2016 12:09 PM | |
Posts: 45 Rating: (1) |
Hello! I fail to see the hardware configuration of my PLC (signal modules and other) online or offline. I have a CPU 1214C AC / DC / RLY (6ES7 214-1BG31-0XB0, V3.0) that was program with TIA Portal V11, which works very well, but my problem is: When I log in as described below: 1- boot tia portal v11 2. Creation of a new project 3- add the hardware configuration -> CPU - >> 6ES7 214-1BG31-0XB0 <- ok create the project with the selected cpu. When I go online, 1- I see nothing but the cpu I configures2- I can load or download the program blocks but I do not see the configuration of other modules (Communication module, SM, ...) which are connected on the CPU in order to change address if needed. I even changed the procedure of adding the hardware configuration by choosing the unspecified CPU (6ES7 2xx-xxxx-xxxx) and I see: (Communication module, the CPU, a signal module, not the other SM) and when I manually added the other, I get the default on all modules. see images attached help me AttachmentTEST HGG.zip (76 Downloads) |
Last edited by: gmt86 at: 4/13/2016 12:25:30 PMLast edited by: Min_Moderator at: 4/13/2016 1:19:41 PMChange formatting |
|
4/13/2016 1:24 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on